Other Parts Discussed in Thread: TPS40140
I have created a design for the TPS40140 using SwitcherPro Online 3.17.
VinMin: 11.4V VinMax: 12.6V Vout: 1.5V Iout: 10A Vout2: 900mV Iout2: 18A
I found a few problems:
The RT resistor (R14) is shown as 127ohm. It should be 127k
The UVLO resistors are shown as 10k & 10k. This would result in a startup at 4V which is too low. They appear to be not calculated.
The ripple current (peak to peak) chosen is quite high, 4.7A for output 1 and 8A for output 2.
The resistors on CS1 and CS2 are always 10k (R1, R2 R30 and R28). They should be calculated from the inductor specs.
The current Limit threshold is displayed as 10A for both outputs. Designing with a different max output current does not change this value or change the ILIM resistor values at R15 and R16. Changing the inductor does affect the ILIM resistors.