This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-EM-CC35X1: Help with Simple Link Wi-Fi Toolbox

Part Number: LP-EM-CC35X1
Other Parts Discussed in Thread: LP-XDS110

Tool/software:

Hello everyone, I'm having troubles with  LP-EM-CC35X1.

I just bought LP-XDS110 and I still cant upload firmware or test the LP-EM-CC35X1, I downloaded Simple Link Wi-Fi Toolbox and the board is not avalailable to select.

Following the LP-EM-CC35X1 guide it says this 

The version of Wi-Fi toolbox I'm using is simplelink_wifi_toolbox_2_2_5

Any help would be great, Thanks in advance.