Part Number: UCC28710
Other Parts Discussed in Thread: UCC28C42
Tool/software:
Hi Expert,
Customer R&D design below schematic, pls help review it, thanks in advance.
Vin=85V, DC
Vout = 12V;
Load = 2A;
ripple = 1% of output;

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Functionally your schematic looks correct; however, the UCC28710 was designed for an output regulation of +/- 5 %. 1% output ripple might be too aggressive.
Also, your design looks to require 14 % duty cycle. The controller was design to operated from a Dmax of 42.5% and peak current and frequency modulation to control the duty cycle. This is what is know as a control law profile.
I reviewed the control law and your design will be operating at a frequency of roughly 33 kHz. This is at the edge of the AM and FM band.
Fmax/dmax = 100 kHz/0.425 = fx/0.14, fx =32.64 kHz
It is recommended that when design with this device to avoid sub harmonic oscillations the frequency at nominal max load be > AM frequency + 10 kHz = 33 kHz + 10 kHz = 44 kHz. Since this design cannot accomplish this you might want to choose another controller for your buck converter.
Since your output ripple requirement is 1% and your design could have subharmonic oscillations I would not recommend using the UCC28710 for your design.
You might consider using a UCC28C42 for your application. You will require a gate drive transformer to drive the high side FET.
Regards,