This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010266: Blood pressure monitoring Circuit

Part Number: TIDA-010266

Tool/software:

Dear TI,

My end goal is to build an accurate and simplified Blood pressure monitoring system,

As part of that I came across TIDA-010266 design circuit, it has some interesting feature which meets my requirements..

As I'm a beginner could you please clarify few queries below:

1. Are there any advanced ICs for BP measurement which reduces circuit complexity ? 

2. Do we have the pump related information ?

3. As you can see in the design guide figure 3-1 what is that yellow colour one which looks like motor and why there are 4 connections to the valve where all connections merged ?

4. Does the controller used in the board is pre-programmed ?

5. Can we use other TI controllers as per requirement ? If yes, please provide any controller interface related information.

Best regards,

Tex