Part Number: PMP41063
Other Parts Discussed in Thread: UCC28730,
Tool/software:
Hi experts,
I'm promoting UCC28730 and ask the customer to refer PMP41063.
The customer notice the L1/L3 have 250VAC rated voltage.
That reference design input voltage reaches 1,000V input so it is out of rated voltage.
Are there any suitable reason to use 744821201/744821110?
Thanks and regrads,
Tsuyoshi