This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563257: TI Pspice older version

Part Number: TPS563257


Tool/software:

I just installed Pspice for TI; it wont open some project files (with schematics) I created from several months ago in a previous version of TI Pspice.

A window pops up and asks if I want to convert them to the current version and when I click OK, it reports that it is not able to convert a 'Capture 9.2.3' version project and just creates a blank project.

The version I installed now is 23.1-2024 S001

Is there something I can do to recover/restore these files / schematics? Should I reinstall the older Pspice version assuming it is available?

---Marcello