Part Number: LM5171-Q1
Other Parts Discussed in Thread: LM5171, LM5171EVM-BIDIR
Tool/software:
I am designing a boost circuit using the LM5171 to boost an input voltage (Vin) of 5V to 12V. I am using an external VCC supply (up to 12V) connected to the Vin pin, along with an external MOSFET. My concern is: when Vin drops to 5V, the VCC supply also drops to 5V. Since I read that the internal LDO in the LM5171 requires VCC to be at least 6V to operate properly, will the LDO still be able to drive the external MOSFET effectively to generate the required voltage for VCC? Could you clarify the LDO's operational requirements and suggest any improvements to ensure reliable operation when Vin is 5V?