Part Number: LMG3422EVM-043
Tool/software:
Hello,
I have 3 Questions:
1. Why are two different isolators used for the High and low side in the daughter card to drive the FETS?
2. Can you please help me understand why these nets are not connected? specifically pins 1, 16. I see the same in the PCB doc when I update teh changes from the schematic to the PCB doc.

3. I am not seeing the source nets for 5V_H and 5V_L. Is there something I am missing? Are we not violating the isolation if the source of the 5V is the same ground reference on primary and secondary side?