Part Number: LP-MSPM0G3519
Tool/software:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP-MSPM0G3519
Tool/software:
Hi Hideki,
What specific part are you referring for the PCB outer diameter? Are you talking about the diameter from the wholes where the plastic leg goes? Or the diameter of an specific pin or via?
Best Regards,
Diego Abad
I want to know the numbers in this diagram
- Outer length, x and y, in mm
- Hole diameter and distance from corner

Hi Hideki,
Thanks for clarifying. The X is around 58.6mm, the Y is around 146.4mm, and the hole size is 3.175mm. The distance from the top to the center of the hole is around 1.905mm, and from the right side to the center of the hole is 2.51mm