Part Number: TPS7H4001-SP
Tool/software:
Considering the following conditions (please, view the schematic image attached), it can be observed an instability in the inductor's current at 3ms where it can be found a value of around 7 A. It occurs only at this time after simulating for 100 ms. Please can you advise us if it is an instability we need to mitigate (or if we need to modify something in our design), or if this is an expected behaviour during the simulation?