Tool/software:
Hi,
I am design and testing a three-phase inverter design based on TIDA-01606.
I have a question regarding the Power Ground Plane and MCU Ground plan:
In the TIDA-01606 design the MCU GND connect to Power GND by a ceramic cap 2200pF, what is the purpose of this connection? what if we isolate MCU GND and Power GND completely, no connection?
Why the designer do not use negative point of DC link voltage (DC-) as Power GND?
Can we select negative point of DC link voltage (DC-) as Power GND and connect with MCU GND directly?
Thank you.