This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS552872-Q1: Stability Plots

Part Number: TPS552872-Q1
Other Parts Discussed in Thread: TPS552872

Tool/software:

Hi All,

Please provide Stability plots for the below Part in the given conditions.

1.Buck-Boost converter, TPS552872
For the following conditions,
Cout= 189uF
Cin = 20.33uF
Lout = 10uH
DC resistance of Lout = 23 mohm
Vin = 9 to 32V
Vout = 12.6V
Iout = 1.681A
ESR of Cout = 1.273mohm
Freq = 1.869MHz 

Thank you.