This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS628501-Q1: Stability Plots

Part Number: TPS628501-Q1
Other Parts Discussed in Thread: TPS628501

Tool/software:

Hi All,

Please provide Stability plots for the below Part in the given conditions.

Buck-Boost converter, TPS628501:


For the following conditions,
Cout= 44.74uF
Cin = 17.28uF
Lout = 470nH
DC resistance of Lout = 37.61 mohm
Vin = 3.333V
Vout = 0.75V
Iout = 504mA
ESR of Cout = 4mohm
Freq = 2.25MHz

Thank you.