Tool/software:
Hi team,
Our customer plan to refer to PMP30446 design to build a board,
and refer to the BOM list.
Customer need more detail information of L2 and T1,
Such as wire diameter, number of turns, core, etc.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi team,
Our customer plan to refer to PMP30446 design to build a board,
and refer to the BOM list.
Customer need more detail information of L2 and T1,
Such as wire diameter, number of turns, core, etc.
Thanks
Hi Roy,
I attach here the datasheets of L2 and T1.
Unfortunately Wuerth cannot disclose the internal structure (type of wire, number of turns, type of core and winding arrangement) because they designed these magnetics and supplied free samples to us. Of course, if they disclose these data, anybody can produce them with other vendors, and their work is lost.
Regarding the inductor, I add here the specifications I sent to Wuerth for the design. Maybe your customer can use it to develop this inductor with their preferred vendor.
PMP30366 Rev_A Buck Inductor.pdf
Best regards,
Roberto