Tool/software:
The power-good (PG) pin is an open-drain output that indicates (short) when the module has no fault and the output voltages are within ±10% of the output voltage regulation setpoints.
i will be using 3 phases, so I need a total of 6 ICs(UCC14141-Q1) since two ICs will be used one phase (High Side / Low Side).
If I connect the PG pins together, it might be difficult to determine which IC is causing an issue if a problem arises. However, I want to use the PG pins in this manner by connecting them together.
1. I'm wondering if it's possible to connect all 6 PG pins together for use.
(The control board will receive the PG input through a single wire.)
2. If it's difficult, is it possible to use two PG pins grouped together on one phase (HS/LS)?
Thank you