This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2844: Inquiry About SMPS Development and Suitable ICs

Part Number: UC2844
Other Parts Discussed in Thread: UCC28951, UCC28950

Tool/software:

Hello,

I have a question regarding SMPS development and the related specifications, as well as possible IC options.

The specifications are as follows:

Multi-output Flyback Converter

Input Voltage Range: 250V ~ 1000V
Control Output Voltage Range: 24V or 5V
Output Power: Approximately 300W

We are planning to develop an SMPS with the above specifications for mass production in our company.

Could you recommend any suitable ICs for this application? If available, please provide the IC datasheet along with the application note.

Thank you.