Part Number: TIDA-00364
Tool/software:
Hi Pawan,
How to calculate motor phase current when 15kW motor and battery is 48V?
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-00364
Tool/software:
Hi Pawan,
How to calculate motor phase current when 15kW motor and battery is 48V?
Best regards,
Hi Forklift,
Please refer to these threads for the details about it:
In case of 15kW, it means the motor current could be up to over 300Arms with a 48V battery:
Input power = 33Vrms x 300Arms x 1.732 x 0.875 = 15kW.
Here, the 0.875 is the assumed power factor, cos(φ), of the ACIM.
Best regards,
Jerome Shan