Other Parts Discussed in Thread: LM5022
Tool/software:
Hello:
There seems to be some reasons for confusion here: looking at PMP21738 design, the loop bandwidth is plotted as having cross-over freq as 110kHz.
Is that possible with LM5022 controller?
And the schematic looks strange with AC rect connected at the output
Can this topology be scaled with a narrow DC input of 26-30v and step-up to 120V @ 300W? Will be using GaN in the primary as well as sync rec with UCC2416 or equivalent MPS68xx
Is there a close matching controller in TINATI ?
Or a SPICE model ?
Appreciate any help in the matter.
r