Tool/software:
Following up on this question. There are these 3 capacitors that are missing on the board/pcb files and missing in the BOM. I can't seem to know what they are purposed for and if they are needed for the core function.
![]()
![]()
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Following up on this question. There are these 3 capacitors that are missing on the board/pcb files and missing in the BOM. I can't seem to know what they are purposed for and if they are needed for the core function.
![]()
![]()
Hello,
Yes this is important part of the design - these are CDLink capacitors.
The capacitors are mounted on the small PCB part located in bottom on the PCB. You need to cutout the piece of PCB and solder capacitors to the piece. Than solder the piece to place shown in your picture abowe. You can use just small 6 pins bended pins to solder them.
Here they are in BOM:

Best regards, Seva.