Part Number: UCC28950
Tool/software:
Hi TI experts,
I am intending to use UCC28950 for a PSFB converter application which serves as a constant current source.
1. Is this chip (PSFB) suitable for power range in 2.4 - 4kW?
2. Is there a way to reliably tune the control loop for both CC and CV control such that there is no overshoot and minimal ripples?
3. During operation, the current reference will be changing between anything that is within 0 - full load. Is this topology still suitable?