Other Parts Discussed in Thread: PMP8740
Tool/software:
hi sir
we would like to design a power supply ,spec as below, could PMP40766 can achieve it
thanks

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Chen Alex1,
Since the total output voltage range needs to go from 0.1V up to 50V and 10mA up to 10A, my recommendation is to use an isolated DC/DC topology that is better suited for wide output voltage range. I would suggest to use PMP8740 as a reference. You wont need such high power but PSFB topology is capable of much wider operating range compared to LLC (the PSFB in PMP8740 is designed for 0V to 32V for example).
https://www.ti.com/tool/PMP8740?keyMatch=pmp8740
Best Regards,
Ben Lough