Other Parts Discussed in Thread: TPS7H4002-SP
Tool/software:
What is the ꝊJA (°C/W) for part number TPS50601A-SP? The datasheet only gives Ta, Tj, Ꝋjc. I need the ꝊJA (°C/W) for analysis so I can use it in a new design.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
What is the ꝊJA (°C/W) for part number TPS50601A-SP? The datasheet only gives Ta, Tj, Ꝋjc. I need the ꝊJA (°C/W) for analysis so I can use it in a new design.
Hi Heather,
Unfortunately we do not have a RθJA for the TPS50601A-SP, only RθJC(bot) as shown in the data sheet.
While not the same device, the TPS7H4002-SP uses the same ceramic package, and has a RθJA value of 25.0 °C/W. Since the devices use the same ceramic package, this number may be a "ballpark" estimate. It is important to note that the actual RθJA for the TPS50601A-SP will be different.
Please see our Application Note "Semiconductor and IC Package Thermal Metrics" for more detailed information on usage of thermal metrics.
Thanks,
Andy