This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00299: SPI use of TIDA-00299

Part Number: TIDA-00299


Tool/software:

ALL HI

Looking at the design guide for TIDM-000299, I see two SPI rates listed in Table 3: 16MHz (slave) and 48MHz (master).

For the use of such a high rate in the SPI hardware design of what matters need to pay attention to? For example, PCB design, EMC, etc. TI has instructions on this design? Thank you.