This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256403: UCC256403

Part Number: UCC256403

Tool/software:

Hi, 

Iam using  UCC256403 IC in my design for LLC converter.

My design input is 350V-420V Voutput is 40V to 60V.

When i opearate with Dc input 390V and output is buillding 55V.

I am observing the audible noise when it is on noload. This noise is increasing when load is applied.

I have attached waveform. Please have suggest what could we can do.