Part Number: TIDA-01606
Tool/software:
Hi,
I have a couple questions related to the updated schematics of the TIDA-01606 Development Board.
- I see you changed from a nonisolated sensing differential amplifier to an isolated voltage sense circuitry on PCC Voltage Measurement E7. Can you please explain why?
- The Capacitors being used as Y-caps C77, C78, C79 are only 630V rated. Is this due to the Capacitor divider reactance @ 60 Hz input?
- What is the purpose of the NTC Voltage Divider and reference on the IsoM5-275-B-L2? Why did you not use a 525V rated MOV and instead used a 275V MOV in series?
- Why are you creating a neutral AEF_CHK_N, and V_PCC_N and V_SN_N rather than providing a single capacitor to GRID_GND?
- C458, C459, C260 are those AC Hot loop capacitors in your design? If that is the case, then why do they not exist on VDC+ and VDC_MID?
- U54 was not on the previous design. Is this to improve the splitting of the CLK to ensure timing is more consistent with the data being received back from the Hall Effect Sensors?
- I am assuming that C67, C71, C72, C73, C75, C76 are used as a AC Coupling capacitor between the Midpoint and the Virtual Neutral of the V_SN_N
Thank you,
-Noah