Part Number: AFE7950EVM
Tool/software:
Good Morning
I have the AFE7950EVM-revA board connected to the TSW14J57-revE board.
I tried to configure the AFE by GUI from Latte tool with the following parameters:
In the Interface Rate menu it allow to you to select two different rate, 819.2MHz and 983.04MHz:
The first one, 819.2MHz, its ok and I can configure without errors.
If I select the second one, 983.04MHz, the tool give me errors and cant configure nothings with this rate.
Why Can I select the second one and nothing can be configure with this rate?
What is the reason?