This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55289: TPS55289

Part Number: TPS55289


Tool/software:

Dear TI's team members,

Driving Condition for Buck-Boost PWM IC :

Input Voltage = 12V

Output Voltage = 6.5V ( +/-5% )

Load Current (max.) = 1mA ~ 4A 

Voltage Ripple = (+/-) 325mV

Could you provide us some feedback about this gain margin & phase margin based on TI's SPICE modeling ?

Thanks & Best Regards !!