This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP23421: recommended transformer for around 3W

Part Number: PMP23421
Other Parts Discussed in Thread: PMP23431, PMP22288

Tool/software:

Hi experts,

Would you tell me the recommended transformer part number (or recommended turn ratio) for following requirements.

PS: 200~320 V(may ~400 V)

SR: 12V/~200mA

Thanks and regards,

Tsuyoshi