Part Number: TIDA-010232
Tool/software:
Hello
I have a question about the TIDA-010232 reference design TIDUEZ8C.
The formula for calculating the time constant of an RC circuit is given as (15)
τ = RisoP//RstP × CisoP
but I would like to know if this is the formula.
- Is it necessary to include RisoN and CisoN in the calculation formula ?
- The conditions state that RisoN is small and RisoP is high, but for example, what values are these set to ?
- Are there any other conditions under which equation (15) holds ?
Best regards