Other Parts Discussed in Thread: TLV1805, TIDA-010239, TINA-TI
Tool/software:
Hello,
I am currently conducting research on electric vehicle (EV) charging, with a particular focus on AC charging communication (J1772, IEC 61851-1) between EVs and charging stations.
I am very interested in your "AM62-EVSE-DEV-PLATFORM" product, and I would also like to ask for your recommendation on the most suitable product for my research purposes.
My goal is to build a testbed that simulates the AC charging process between an EV and an EVSE, based on the IEC 61851-1 protocol. For this, I require both an EV-side and an EVSE-side board, and the system must be capable of handling the entire charging scenario, including PWM signal communication and charging state transitions.
I believe your products are well-suited for this purpose and am considering a purchase. However, before making a final decision, I would like to confirm a few details as outlined below:
Having reviewed your offerings, I believe your development platforms may be well-suited for this purpose. However, I would like to clarify a few points before proceeding with a purchase:
1. Suitability for Research Testbed
The primary objective of my testbed is to observe how PWM signal voltage and duty cycle affect maximum charging current and state transitions during AC charging (J1772, IEC 61851-1).
Could you kindly confirm whether the above-mentioned boards are capable of supporting such functionality?
In case these boards are not suitable for this specific use case, could you recommend alternative boards or development kits from your portfolio that would meet these requirements?
2. Real-Time Observation of PWM Signals
I plan to measure the PWM signal's voltage level and duty cycle in real time using an oscilloscope.
Could you confirm whether the PWM signal generated by your boards is accessible via external signal lines for such observation?
Thank you very much for taking the time to review my inquiry.
Your response will be highly valuable in helping our research team make an informed decision regarding our development platform.