This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5146: 2-phase Buck converter simulation doesn't look as expected.

Part Number: LM5146
Other Parts Discussed in Thread: LM5145-Q1, LV5144, , LM5145, LM5149-Q1EVM-400, LM5149-Q1, LM5148-Q1, LM5149, LM5148

Tool/software:

Hello,

I am trying to develop a 13.5V, 40A buck converter. For the same, I decided to go with LM5146 in a 2-phase configuration with each phase carrying 20A. 

Initially I tested with 1-phase and things are operating as expected. But with the 2-phase design, the things seem to get a bit wonky with the Output Voltage and Current. 

I have added all my material at this link: Buck_Converter. I am hoping for some expert advice on this. 

PS: My input voltage range is 30V to around 95V. I am also looking to develop this design to be pin swappable with LV5144, LM5146-Q1, LM5145, LM5145-Q1 based on different Vin(max) requirements.