This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8329EVM: MCF8329EVM: MCF8329EVM: EVM can't dirve BLDC motor

Part Number: MCF8329EVM
Other Parts Discussed in Thread: MCF8329A

Tool/software:

Hello. I am currently trying to drive a BLDC motor using an EVM. However, when using the initial configuration file "Default Register MCF8329A.json" found from E2E to run the MPET function, the motor does not operate and instead produces a high-pitched noise. Additionally, within Motor Studio, the "Run MPET" button for the MPET function is completely disabled and cannot be clicked. The EVM hardware settings were configured according to the guide.