This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010054: Controller file

Part Number: TIDA-010054
Other Parts Discussed in Thread: TMDSCNCD280039C,

Tool/software:

Hi,

I want to simulate the TMDSCNCD280039C controller in TINA or PLECS software.

I am planning to integrate the controller in the simulation.

so, can you please share the HDL file of the controller.

Can you please share any suggestion which software is better for integration.

  • Hi,

    Thanks for reaching out.
    I highly recommend PLECS for the simulation of a complete power converter like TIDA-010054.
    We have a PLECS simulation deck available on the reference design page, which can be used as a starting point.

    Also PLECS has libraries which support C2000 code generation and hardware in the loop tests.
    We did not do this with TIDA-010054 specifically, but the all the tool are available.

    You can find some instruction on C2000 +PLECS here: www.plexim.com/.../c2000manual.pdf

    Best regards,
    Andreas