Other Parts Discussed in Thread: TPS26750
Tool/software:
Hello,
I am currently reviewing the TIDT407 document (Test Report: PMP41115 240W USB Type-C® and USB PD 3.1 Charger Reference Design), and I have two questions that I’d appreciate your feedback on:
-
According to the TPS26750 datasheet, the PP5V pin should be supplied externally with 5V/3A to enable OTG mode operation at 15W (5V/3A). However, the PMP41115 reference design uses an LDO (TPS7A2450) with a maximum output current of only 0.2A, which does not meet the 3.6A recommendation from the datasheet. How does PMP41115 achieve 15W OTG mode output (5V/3A) under this architecture?
-
On page 14 of TIDT407, Figure 3-8 is labeled as “5V/3A Output, Start-Up Waveform”, but the waveform shown appears to be from Figure 3-9, which is “OTG Mode, 50.4Vbat, 9V/3A Output, Start-Up Waveform”. Has there been an updated version of the document with the correct 5V/3A output startup waveform?
Thank you in advance for your support.