Part Number: LMR33630
Tool/software:
Hi TI supporter,
I'm designing the -5V circuit but don't know whether it work or not.
Can you please help to review my circuit?
Thank you so much.
Long Le Nguyen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Long,
The one concern I see with the design is the inductor current rating. TI recommends that your inductor saturation current rating is at least as high as the high side switch current limit of the device to avoid significant saturation. In an inverting buck boost, the current stresses are more important to note. Please see section 4.2 in this application note that gives more details about this.
Thank you,
Joshua Austria