Part Number: PMP23126
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hi team,
I used the PMP23126 solution under C2000Ware_DigitalPower_SDK_5_05_00-00 for experiments. I imported the models separately using MATLAB 2024a and MATLAB 2024b, and found that the Simulink model files inside could not be opened, resulting in the following error:
'/MATLAB Drive/matlab_TIPSFB/PMP23126_host_model_OpenLoop.slx' 不是有效的 Simulink 模型文件: Could not open source package
The other model files also reported the same error. May I ask if this is because the published file is encrypted or damaged, or if there are other reasons that prevent it from being opened?
thank you!
Best regards,
Jiahui