Part Number: PMP23377
Other Parts Discussed in Thread: LM51770, LM5177,
Tool/software:
Hi all,
My customer is considering using LM51770 between battery and motor driver in the following configuration.
Vin=48~56V(Vbattery)
Vou=48V
Iout=20A
I found PMP23377 to refer to reference design. I would suggest this, but LM5177 is used.
1) Can LM51770 be used instead of LM5177?
2) Are there any other devices or reference designs you would recommend for the above configuration?
Best Regards,
Ryusuke