Part Number: PMP21943
Other Parts Discussed in Thread: LM5170, BQ25756E, TIDA-00195
Tool/software:

Hello Dears,
I looked at your sample designs PMP21943 and TIDA-0104x and I want to try to build a tester (charger/discharger) for LiFePo4 batteries with a charge/discharge current of 300A based on them. The input power supply is 12V/125A. Please advise, can I use IC LM5170 with an external driver to control an IGBT module (1200V/450A)? Do I also need to use a specialized chip like bq25756E?
Regards,
Tsvetan Ginin