Part Number: LM5025
Tool/software:
I am trying to undestand how the maximum duty cycle on the LM5025 works. I currently have a forward converter with a base clock of 200kHz configured using RT and a 225kHz clock being fed into the sync pin with a 50% duty cycle. What are the requirements on the LM5025 to implement a maximum duty cycle as described under the "Oscillator and Sync capability" in the datasheet?