Part Number: PMP10783
Tool/software:
Good day Sheng-Yang.
Am designing a buck converter input voltage 80V to 120V and an output voltage of 51V, output current of 0.5A using the PMP10783 reference design. Please advice me on how I can go about powering the UCC28C42D since the output voltage is way above the recommended 20V for VDD? I think I will have to use an 18V zener diode.
I await your advice.