This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP41037: Question about PMP41037

Part Number: PMP41037
Other Parts Discussed in Thread: TIDA-010062

Tool/software:

Hi teams,

My customer Lango has a new power supply case and is evaluating: PMP41037 (1kW, 800V to 12V serial half-bridge bidirectional DCX reference design using GaN and C2000)
The client has downloaded some design files from www.ti.com.cn/.../PMP41037, but the client still needs the following information:
1. Simulation files
2. Incomplete schematics, missing DSP page
3. Missing design guideline document
would we provide these materials to the client?

Best Regards

Chris

  • Hi Chris,

    Thanks for trusting our reference design.

    1, Put my simulation for SHB principle in below.

    2, We don't have create the DSP board, but only made an adapter board to use the existing C2000 cCard. So, you will need refer the schematic of C2000 control card;

    3, This is an subset of LLC design, and only operated on resonant frequency, so can you refer to the LLC design guide in TIDA-010062?

    SHBLLC_openloop.zip