This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28056: UCC28056

Part Number: UCC28056

Tool/software:

I want to design a PFC to meet the following requirements:

Input voltage : 240VAC
Input frequency : 50Hz
Output voltage : 380V DC
Output power : 180W

Please provide a reference design.