This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62903-Q1: How can I simulate the SPICE simulation with TPS62903-Q1 model using Spectre

Part Number: TPS62903-Q1

Tool/software:

I want to simulate the TPS62903-Q1 schematic using Cadence Spectre. But this model was encrypted & made error in spectre simulation environment. (like below)

ERROR (SFE-874): Cannot run the simulation because an error was found in the protected block while reading the circuit. Contact the third-party who provided the protected block to correct it and rerun the simulation.
ERROR (SFE-1815): Cannot run the simulation because an error was found in the protected block while reading the circuit. Contact the third-party who provided the protected block to correct it and rerun the simulation.

How can I simulate the SPICE simulation with TPS62903-Q1 model using Spectre? Is there any solution about this??