Other Parts Discussed in Thread: BQ25756, TPS26750
Tool/software:
Hi,
I was just wondering, will a design similar to PMP41115, which can charge and discharge at 240W through USB-C, work with a 9S battery pack instead of a 10S - 12S one? Pack voltage range is 26.1V to 37.8V. (2.9V/cell low-voltage cutoff)
I can afford to cutoff at up to 3.25V/cell (so 29.25V) without significant decreases in runtime, but no higher, and this would be difficult because I can't find any no-programming BMS chips by TI that offer a low-voltage cut-off this high.
Total pack capacity is 100Wh. Board area can be 10725mm^2, and ideally I would use 4 layers, but I'm ok with 6 or 8 too.
Thank you very much.