Tool/software:
Hi,
I am trying to get the arc fault detection working. When I start the live preview in the model composer interface, i inmediatly seem to detect an arc, even when there isn't any connection with the CTs. Also i don't see anything appear on the plot and the button shows "start preview" inmediatly. WHen looking in CCS in a debugger mode, result.buf0[0] = a negative integer.
WIth kind regards,
Cemil