Part Number: TIDA-010938
Tool/software:
Hi,
I noticed that the on-resistance of the GaN device is 30 milliohms, would it be feasible to replace it with a 70 milliohms product instead
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-010938
Tool/software:
Hi,
I noticed that the on-resistance of the GaN device is 30 milliohms, would it be feasible to replace it with a 70 milliohms product instead
Hi,
Since the on-resistance increases from 30mOhms to 70mOhms, the conductions losses will also increase significantly. This will influence the total losses and power to be pushed through each stage.
Thanks,
Veda