Part Number: TMDSCNCD28P55X
Other Parts Discussed in Thread: TIDA-010955
Tool/software:
Hi, I was looking through this device's design guide and application in arc fault detection using embedded AI models.
This device is composed with TIDA-010955 and control card C2000.
I've trained 3 models at model composer as listed below, using example data provided by TI. (it can be found at 'Arc Fault Detection using Embedded AI models' document, 6.2 Data Uploading)
1. ArcFault_model_200
2. ArcFault_model_300
3. ArcFault_model_700
However, when I tested with just the DC current source into CT (pin J8), model 300 and 700 shows 'arc' at model composer GUI even without the arc generation.
Can you please have a look at those models that whether they work fine in TI's test environment or not?
It would be kind of you if test environment when example data was made can be provided such as inverter's switching frequency... etc.
Thank you for your support.