Part Number: PMP31349
Other Parts Discussed in Thread: LM5148, , PMP31344
Tool/software:
Hi,
I am working on creating a buck converter with 24-60V input, 12V output, 5A continuous with peak of 20A. My basis is going around the PMP31349 reference design. I was wondering on the design, why the SW node of the LM5148 is connected directly to GND, and is not connected to the SW node coming out of the LMG2100 GAN half-bridge. In the design, it is setup to run in only PFWM, and for efficiency concerns, I would like PFM enabled due to requiring light load efficiency,
1) is it possible to connect these?
2) can PFM or diode emulation work with the external FET driver and no SW node connected?