Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hello
I am following the guideline of PMP23338 (https://dev.ti.com/tirex/explore/node?node=A__ANlQ.5FNEOWS7jYnIynC-g__digital_power_c2000ware_sdk_software_package__5C6SEVO__LATEST) and trying to run builds/labs to test PFC operation. To run the build/lab1, I shorted the relay and baby boost and removed R145 and R147. I connected a 12V, changed project options, rebuilt project and run debug as guideline request. When I debug, the expressions looks like this: .
1. I set Lab1 in main.syscfg but the expressions always show lab4 as in picture. No matter which lab I change, the expression just show lab4. I have saved the page before debug. Is that an issue?
2. The TTPLPFC_autoStartSlew is 0 when i run my debug. But in guideline, it said this value should go to 100. What is this value mean and what should I do for now if it is always 0?
3. The guideline in part 6.1 ask to connect 12V and turn it on first, then it said to connect a DC power supply with rating of 100V. I should not turn off the 12V right?
Please help. Thank you very much.