Part Number: PMP30446
Other Parts Discussed in Thread: UCC28C50-Q1
Tool/software:
Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
As part of my project, I'm designing a buck converter using a topology similar to the one in your PMP30446 reference design — a dual-buck configuration with a shared center point. Unlike PMP30446, I’m using the UCC28C50-Q1 PWM controller operating in peak current mode with fully isolated voltage and current feedback. The final application will run from a 1000 V battery and deliver 800 V at 12.5 A (10 kW).
After reviewing the PMP30446 schematic, I have a couple of questions:
1. How does PMP30446 achieve center point voltage balancing?
In the design description, it is mentioned that the center point balances automatically using a single coupled inductor (1:1). Could you please clarify how this works in practice?
Is there any special requirement in terms of layout or control strategy to ensure that the midpoint remains stable during dynamic operation or load transients?
2. What is the purpose of resistors R100 to R107?
In the schematic, I noticed a series of 1 MΩ resistors (R100 to R107). Could you explain their intended role in the design?
3. Can you elaborate on how the voltage feedback is implemented?
Could you briefly explain how the output voltage is sensed and processed for regulation in PMP30446?
Thank you for your help.
Kind regards,
Marvin